Suggestions

    For energy-efficiency gains, let’s get our houses in order

     

    November 11, 2021

     

    Raising the global building renovation rate will cut greenhouse gas emissions and reap multiple rewards.

     

    As COP26 draws to a close, there is an important item still on the agenda. Today, the UN annual climate conference will feature a day fully dedicated to addressing the environmental impact of cities and the built environment- an issue that needs to be addressed urgently.

     

    It’s surprising that this item is so often overlooked, given that our buildings are responsible for 40% of the world’s greenhouse gas emissions. And even within this space, it’s new, zero-energy buildings that make the headlines, with futuristic designs that incorporate cutting-edge technology to perform with the lightest possible impact.

    LED lighting is one of the quickest renovations that dramatically cuts carbon - it does not require large capital investments and has a short payback time.”

     

    Raising the standard of our new building stock will be a welcome change, driven by new building codes that will ensure that construction projects adopt a net-zero standard. But to achieve our ambitious 2030 emissions reduction targets, we must look to the areas where we can make the most meaningful impact. Within Europe, 85 to 95% of our current building stock will still be in use in 30 years’ time. If we focus energy-efficiency initiatives on the small percentage of new buildings, we address only a minor part of the problem.

    Laying strong foundations

     

    At present, just 1% of existing buildings undergo energy renovation each year. If we raise that rate to 3% per year, we can clean up most of our built environment by 2050.

     

    Renovation is a multi-level process with varying levels of complexity, incorporating solutions like insulation, high-efficiency heating and cooling systems, and renewable heat and electricity generation systems. To achieve our 2030 targets, we should prioritise one of the quickest wins: lighting. Energy-efficient LED lighting has been with us for a decade now, yet even in highly-developed Europe, two thirds of installed lighting relies on inefficient legacy technology. For the United Kingdom and Ireland (UK&I) region, switching to LED lighting in the professional lighting market could reduce CO2 emissions by 3.9 million tonnes in, the amount of emissions that 175 million trees could sequester in a year. Making the switch would also generate electricity savings of 16.1 TWh, which is equivalent to the annual electricity consumption of more than 4.3 million households. This would mean a saving of EUR 3.8 billion on electricity costs.

    Brighter solutions

    Brighter solutions

     

    Upgrading lighting is also the quickest and least intrusive part of the renovation process. Converting to smart LED lighting can reduce the built environment’s lighting-related energy consumption by up to 80%, offering carbon emissions reductions and bringing down electricity costs. And when LEDs are connected to a smart lighting management platform, the benefits multiply. A lighting system can be connected to other smart building technologies like sensors that can switch off lights in unoccupied rooms or adjust lighting levels in response to natural daylight conditions. Such systems can yield a 30% electricity saving over and above the savings from switching to LED. To add to the benefits, LED lighting is one of the quickest renovations that dramatically cuts carbon - it does not require large capital investments and has a short payback time.

    Encouraging energy-efficient retrofits in the built environment and better planning new infrastructure development, with a focus on technologies that can expedite reduction of carbon emissions can offer definite results.”

    In the European Union and the UK&I region, the Renovation Wave initiative aims to take on the challenge of upgrading aging buildings to keep our emissions within agreed levels. The initiative aims to double annual energy renovation rate in the next ten years. Such a plan yields multiple benefits, slashing emissions from our built environment while reducing energy poverty, improving quality of life, and creating skilled local jobs. The UK also has a resilience and recovery plan - The Ten Point Plan for a Green Industrial Revolution - which lays out a broad roadmap towards this goal and in particular its financing.

     

    Replicating such a scheme globally will undoubtedly be challenging. But with so much at stake, and with quick and significant additional gains on the table, it’s high time for our built environment to take its place on the world’s most important agenda.

    About the author:

    Harry Verhaar

    Stephen Rouatt

    CEO, Signify UKI

     

     

    For further information, please contact:

    Signify Corporate Communications
    Nikita Mahajan

    Tel: 07459751618

    Email: nikita.mahajan@signify.com

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. With 2020 sales of EUR 6.5 billion, we have approximately 37,000 employees and are present in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We achieved carbon neutrality in 2020, have been in the Dow Jones Sustainability World Index since our IPO for four consecutive years and were named Industry Leader in 2017, 2018 and 2019. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.

    Meydan Bridge

    More blogs

    • Ultra efficient bulb for planet and purse

      October 19, 2021

      Ultra efficient bulb for planet and purse

    • UV-C from Supermarkets to Stables

      September 21, 2021

      UV-C from Supermarkets to Stables

    • Disinfecting the air we breathe with UV-C light

      June 21, 2021

      Disinfecting the air we breathe with UV-C light