Be the first! Get the latest news and updates
Suggestions

    Study Finds Philips LED Lights Provide Improved Energy Efficiency and Production for Growing Food Crops in Space

    March 22, 2016

    • University of Arizona and Philips Lighting collaborated to create improved lighting for plant production in Mars-lunar greenhouses
    • Non-water cooled LED lights used 56% less energy; more than doubling production of edible biomass per kWh compared to previous water cooled high pressure sodium system
    • Research findings to inform development of new innovations in urban farming


    Somerset, NJ – March 22, 2016 – Philips Lighting, a Royal Philips (NYSE: PHG, AEX, PHIA) company and global leader in lighting, has collaborated with The University of Arizona Controlled Environment Agriculture Center (CEAC) to test energy efficient ways to grow food that will help feed astronauts on missions to the moon, Mars and beyond. A recent study, conducted over a nine week period, found that replacing water-cooled high-pressure sodium (HPS) systems with energy efficient LED lighting from Philips in a prototype lunar greenhouse resulted in an increased amount of high-quality edible lettuce while dramatically improving operational efficiency and use of resources.  Lettuce grown under Philips LED modules achieved up to 54 grams/kWh of fresh weight, edible lettuce compared to lettuce grown under a high pressure sodium system which achieved only 24 grams/kWh of fresh weight, edible lettuce. This represents an energy savings of 56%.


    “The lunar greenhouses equipped with Philips LED modules provided the light needed to produce the same amount of indoor crops that the specialized water-cooled sodium systems provide while significantly decreasing the amount of electrical energy used,” said Gene Giacomelli, Ph.D and CEAC Director. “Findings from this study are critical in that not only can it be applied to growing food in space but can be applied to farming techniques in places where there is a shortage of water and good agricultural land right here on this planet.”


    Philips GreenPower LED toplighting was installed and programmed with a customized “light recipe” developed by plant specialists at Philips to optimize the results. Light recipes are formulated by taking into account a variety of factors including light spectrum, intensity, uniformity and relative position of the lamp to plant canopy. These are combined to develop specific plant characteristics such as compactness, color intensity and branch development.


    In addition, the LED modules, which create less concentrated heat loads than HPS lamps, even without water cooling, can be placed closer to the plants resulting in uniform light distribution throughout the greenhouse. This ensures all plants receive the same level and quality of light resulting in better, more uniform plant quality and a more predictable yield. The Philips LED systems also cool independently, which means no additional investment is required in cooling water distribution.


    “Dr. Giacomelli and his team at CEAC have been on the cutting edge of pioneering research that is uncovering new ways to grow crops in closed and controlled environments. Results from this study will not only impact growing crops in space but will provide tangible sustainability benefits for indoor farming on our own planet,” commented Blake Lange, Business Development Manager of the Philips City Farming Division. “We know that it is becoming more difficult for traditional farming practices to keep up with the demand for high-quality, locally grown food, particularly in areas of high population density and with local water shortages. The work we are doing is focused on driving innovation of new farming technologies that allow food crops to grow in indoor environments, absent of natural light and in close proximity of cities and major population centers, thus reducing the distance from farm to fork.”


    “NASA has been working with universities for over 25 years to discover how the use of LEDs can support plant growth in closed environments.  Over that time we have used patented LED technology as part of the Astroculture plant growth chambers for the Space Shuttle and the International Space Station (ISS), NASA’s ground based Habitat Demonstration Unit, as well as NASA’s VEGGIE plant unit on the ISS,” said Ray Wheeler, a NASA plant physiologist.  “It is fascinating to see how LED plant lighting has expanded so rapidly around the world and continues to further develop as we have seen most recently with the Mars-Lunar Greenhouse Project at the University of Arizona.”  

    Lunar Greenhouses

    Lunar Greenhouses

    Lunar Greenhouses

    Lunar Greenhouses

    Lunar Greenhouses

    Lunar Greenhouses

    For further information, please contact:

    Melissa Kanter
    Philips Lighting
    Tel: 732-563-3994
    Email:   melissa.kanter@signify.com

    About the Study

    The project was completed over a six month period by a team led by Dr. Gene Giacomelli within the Mars-Lunar Greenhouse created by Sadler Machine Co. During a nine week period, four harvests of lettuce heads weighing 5 to 6 ounces were analyzed.  All plant production and growing practices remained constant between two, distinct growing systems—LEDs with the specially developed light recipes from Philips Lighting versus a traditional high pressure sodium system which included a glass water jacket for removing the concentrated heat from the lamp bulb.

    About the University of Arizona CEAC

    The University of Arizona Controlled Environment Agriculture Center located in Tucson, Arizona is focused on the science and engineering of maximizing plant production within controlled environments. The Mars-Lunar Greenhouse project is a NASA collaboration supported by the Arizona-NASA Steckler Space Grant, which supports university research and technology development activities to achieve innovative research and expanded technology applications.

       

    About Philips Lighting

    Philips Lighting, a Royal Philips (NYSE: PHG, AEX: PHIA) company, is the global leader in lighting products, systems and services. Our understanding of how lighting positively affects people coupled with our deep technological know-how enable us to deliver digital lighting innovations that unlock new business value, deliver rich user experiences and help to improve lives. Serving professional and consumer markets, we sell more energy efficient LED lighting than any other company. We lead the industry in connected lighting systems and services, leveraging the Internet of Things to take light beyond illumination and transform homes, buildings and urban spaces. In 2015, we had sales of EUR 7.4 billion and employed 33,000 people worldwide. News from Philips Lighting is located at www.philips.com/newscenter.