Be the first! Get the latest news and updates
Suggestions

    Philips launches first direct LED replacement range for CFL based downlights with 60% energy savings

    March 7, 2016

    • Targeted at European market of 150 million installed CFLni lamps
    • First click-to-fit compatible replacement without need to replace EM or HF ballast
    • 3x longer lifetime than CFL and more environmentally friendly


    Frankfurt, Germany – Philips Lighting, a Royal Philips (NYSE: PHG, AEX: PHIA) company and global leader in lighting, announces the launch of the first LED retrofit range for compact fluorescent lamps (CFLni) commonly used in downlights. Philips CorePro LED PLC builds on the highly successful Philips MASTER LEDtube InstantFit and uses the same click-to-fit technology for replacing CFLni lamps that work with existing Electro Magnetic (EM) and High Frequency (HF) ballasts. The new lamp will be targeted at replacing the 150 million CFLni lamps found across Europe and provides 60% energy saving over conventional PL-C lamps.


    The Philips CorePro LED PLC range is the first ever retrofit LED alternative to compact fluorescent lamps in down lighting applications that comes in a fully retrofit form factor and offers EM and HF ballast compatible versions. Used for general lighting applications in offices, hallways, staircases, receptions and meeting rooms everywhere, Philips Lighting has reimaged one of the world’s most common lamps used in downlights.  The new lamps simply plug and play into existing fittings without the need for any modifications to the existing lighting fixtures. Philips CorePro LED PLC deliver energy savings up to 60% and has a lifetime that is three times longer than conventional fluorescent PL-C lamps. Installation and maintenance costs are also kept to the bare minimum thanks to simple plug and play installation and the robust, shatterproof plastic housing. The average pay-back time is less than two years.


    “With nearly 150 million conventional fluorescent PL-C lamps estimated to be installed in Europe alone, a direct retrofit LED replacement to this commonly used lamp has been long awaited. The benefits of LEDtubes are now also available for LED PLC lamps with a simple replacement of a lamp,” said Rowena Lee Business Leader LED Lamps at Philips Lighting.


    Notes to editor


    Product benefits Philips CorePro LED PLC

    • The Philips CorePro LED PLC has a three times longer lifetime than CFLs (30,000 hrs) which results in significant maintenance savings. The average pay-back time is less than two years.
    • The Philips CorePro LED PLC enables a quick and easy lighting upgrade, without the need for any modifications to the existing luminaires.
    • Improved light quality with instant illumination and the entire elimination of the flickering associated with conventional fluorescent lamps.
    • The lamps are able to rotate, in order to ensure optimum lighting levels and enabling the distribution of light to be adjusted as effectively as possible to suit the existing luminaires
    • The light emitted from the LED lamps contains no UV or infrared component, so there is no risk of the light causing textiles or other materials to bleach or fade over time.
    • The Philips CorePro LED PLC is available in conventional compact fluorescent lamp lengths in 18 and 26-watt versions and with either a two-pin or four-pin cap, making it suitable for use in lighting applications with conventional or electronic ballasts and compliant with all European regulations.
    • Philips CorePro LED PLC are available now via European distributors in warm white (3,000 K) and natural white (4,000 K) color temperatures.


    Philips Lighting will showcase truly pioneering lighting innovations at Light + Building 2016, the world’s leading trade fair for lighting in Frankfurt, Germany. Please visit our stand at Messe Frankfurt, Hall 0: Forum.

    For further information, please contact:

    Anne-Marie Sleurink
    Philips Lighting
    Tel: +31622306529
    Email: anne-marie.sleurink@signify.com

    About Philips Lighting

    Philips Lighting, a Royal Philips (NYSE: PHG, AEX: PHIA) company, is the global leader in lighting products, systems and services. Our understanding of how lighting positively affects people coupled with our deep technological know-how enable us to deliver digital lighting innovations that unlock new business value, deliver rich user experiences and help to improve lives. Serving professional and consumer markets, we sell more energy efficient LED lighting than any other company. We lead the industry in connected lighting systems and services, leveraging the Internet of Things to take light beyond illumination and transform homes, buildings and urban spaces. In 2015, we had sales of EUR 7.4 billion and employed 33,000 people worldwide. News from Philips Lighting is located at www.philips.com/newscenter