Philips integrated LED indoor lighting range now available in warm white

August 9, 2012

 

Sydney, Australia – Philips Ledino, a complete range of indoor lighting using advanced state of the art LED technology, is now available with a warm white light output that creates a soft, ambient light effect for your living space.

Crafted from high-grade glass and brushed aluminium, each model in the Ledino range is both minimalist and elegant. Simple and versatile, the Philips Ledino range injects a natural sense of purity and beauty into the home. Designed for maximum efficiency, the directed light source means little light is lost through spillage.

LED is highly energy efficient, saving up to 80 per cent of energy compared to traditional light sources1, but with a comparable amount of light. The 7.5W lamp has a light output similar to a 40W traditional incandescent bulb. Furthermore, the Power LED integrated into the Ledino range performs at its peak for up to 20,000 hours, so there is no need to ever change a light bulb.

“Philips is spearheading LED innovation with the introduction of warm white LED, which give a soft, warm and natural light output, ideal for an ambient home environment,” said Michael Downie, General Manager of Philips Lighting Australia. “The energy efficiency of LED means that with a Ledino lamp, you can create a warm ambient feel in the home, for just a fraction of the energy consumption.”

Elegant, linear designs together with an integrated LED light source make Philips Ledino lamps ideal for any room in the house, including the kitchen, dining area, living room or bedroom.

 

Philips Ledino ceiling light
This modern, two or three-light flat panel rectangular ceiling light provides powerful, warm white light from a single sheet of polished aluminium. Its pure, understated design blends in to the ceiling and also adds a touch of contemporary style to any room.


RRP: $169.95
Energy consumption: 22.5W

   

 

 

Philips Ledino wall light
This rounded and appealing dome sits discretely on the wall and casts a diffuse glow of ambient light from its smiling mouth. Available in both white and grey aluminium.


RRP: $84.95
Energy consumption: 5W

   

Philips Ledino spot lights
Four individual spot lights are mounted on a 360 degree turning circle, so light can be directed precisely where it is needed with a simple turn of the wrist. It comes in one, two or four spot in white aluminium.

 

RRP: $89.95 (for one spot); $149.95 (for two spots); $229.95 for four spots)
Energy consumption: 7.5W (for one spot)

   

 

 

Philips Ledino downlights

A set of three pinpoint recessed spots so tiny that they’ll fit anywhere without altering the look of your home. Complete with a diamond-studded light so bright and sparkling it will make a great design feature in its own right. Available in white or brushed aluminium. 

 

RRP: $89.95
Energy consumption: 22.5W

 

 

 

 

Philips Ledino downlight

The individual recessed downlight may be compact, but the light is provides enough lighting to illuminate any space, ensuring the only attention-grabbing thing about your lighting system is its pure, bright light. Available in white or brushed aluminium.

RRP: $99.95
Energy consumption: 7.5W

   


The Philips Ledino warm white range is available at Lights For You stores in NSW, and from selected lighting specialist stores in Victoria and Queensland. The range is also online at www.lightsforyou.com.au.

 

 

1 Incandescent lamps

About Royal Philips Electronics

Royal Philips Electronics of the Netherlands (NYSE: PHG, AEX: PHI) is a diversified health and well-being company, focused on improving people’s lives through timely innovations. As a world leader in healthcare, lifestyle and lighting, Philips integrates technologies and design into people-centric solutions, based on fundamental customer insights and the brand promise of “sense and simplicity.” Headquartered in the Netherlands, Philips employs approximately 122,000 employees with sales and services in more than 100 countries worldwide. With sales of EUR 22.6 billion in 2011, the company is a market leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as lifestyle products for personal well-being and pleasure with strong leadership positions in male shaving and grooming, portable entertainment and oral healthcare. News from Philips is located at www.philips.com/newscenter..

We'd love to hear from you