With a menu that changes according to the four seasons, owner Cheng Hsin Yao researched and looked around for the most natural source of ambient lighting solutions, that could amp up the dining experience, by giving out light like passing clouds in the day to rosy sunsets and starry night skies.
Bright ideas came alive when restaurateur Cheng Hsin Yao and his architect and designer, Felicia Toh of Quarters Design Studio, envisioned a place which could offer the best of both worlds: the liveliness and exuberance of outdoor dining in a much-appreciated air-conditioned indoor environment set within a mall on the sunny island of Singapore, which is hot and humid all year round. The challenge they had was how to transform an indoor space within a shopping mall to mimic an outdoor park, which requires a lot of natural ambient light. Moreover, the deep floor plan of the existing Wisma Atria unit, which only had windows along one side, and the relatively low ceiling height made it difficult to achieve the concept.
"We wanted to create an atmosphere where nuances of street scenes could be distilled within the space—moving traffic, cloudscapes, floral fields. We imagined viewing these scenes through ‘window frames', and suspended overhead from the ceilings, so the atmosphere of the exterior would envelop the interior space.
We were excited when we found that Color Kinetics Luminous Textile could recreate softly nuanced and abstracted imagery within the space, without causing glare, which was ideal for the restaurant since diners would be sitting very close to these panels," explained Felicia.
To turn this vision into reality, Hsin Yao and Felicia passionately worked with Signify Lighting Design specialists to specify innovative and beautifully designed lighting solutions for this project.
A high-performance luminaire, Color Kinetics PureStyle was the perfect choice for illuminating Picnic's alcoves and accent spaces. Its innovative, aesthetically pleasing form factor fit seamlessly within the application areas. Color Kinetics ColorBurst Powercore LED spotlights were also used as accent lights along the food street, cast artistically on the colorful food trucks.
Project credits
Architect:
Felicia Toh, Architect and designer, Quarters Design Studio
January 23, 2024
The Evolution of Healthcare Lighting
November 14, 2023
How lighting technology can help reduce risks to migrating birds
September 15, 2023
Unlocking America’s energy efficiency potential